Proxim Wireless Announces Enterprise-Class 802.11ac Wi-Fi Adapter

Proxim

Silicon Valley, CA, March 30, 2015 – Proxim Wireless Corporation (OTC Markets: PRXM), a pioneer and global
leader in advanced Wi-Fi, point to point (PtP), and point to multipoint (PtMP) radio systems, today announced
the launch of the ORiNOCO® USB-9100 Wi-Fi Adapter with dual-band 802.11a/b/g/n/ac support, enabling users
to experience next-generation, ultrafast Wi-Fi access.

Based on the latest IEEE ratified standard - 802.11ac, the ORiNOCO USB-9100 wireless adapter allows high speed
Wi-Fi access from 11ac access points and routers to notebook or desktop computers. The dual internal antenna design gives enhanced wireless network coverage, while the advanced MIMO technology delivers improved system throughputs even
in dense office environments. 

The feature-packed ORiNOCO USB-9100 adapter also boasts a ‘superspeed’ USB 3.0 interface for seamless data transfers between the adapter and computer, without compromising on security with advanced WPA2 protected access. Additionally, the compact and sleek design reduces desktop clutter, making it ideal for enterprises and homes alike. These enterprise-class features of the ORiNOCO USB-9100 will enable this product to stand out from competitive but consumer-class offerings. 


Read the Complete Press Announcement

Related