Raritan Introduces High Performance, IP User Station for Broadcast and Control Room Operations

 Industry’s most productive and powerful user interface to view, access and control workstations and servers remotely. 

Schiedam, Netherlands - 7 January, 2016Raritan, a leading provider of intelligent data center management, KVM and rack power distribution solutions—today introduced a new IP User Station for the Dominion® KX III digital KVM switch.  Together they provide technicians, operators, engineers and IT professionals with an economical IP-based solution for high-performance remote access to IT devices with the industry’s most productive and powerful user interface. 

Ideal for the work done in broadcast studios, control rooms and labs, as well as offices and data centers, the KX III User Station solution supports: two 1920 x1080 video sessions at 30 frames per second, sub-second switching between servers, and eight or more simultaneous KVM-over-IP sessions over single or dual monitors. Unlike other high-performance KVM solutions that require a separate network, users can access and control multiple servers and other equipment over the corporate LAN and/or WAN.  Moreover, the KX III’s web-browser interface enables authorized users to access connected equipment using their laptop or PC while traveling or for emergency access from home.

Read the full article here.

Related