T-BERD 5800-100G. All-in-One Handheld Network & Fiber Testing

T-BERD 5800-100G omage

The VIAVI OTDR T-BERD 5800-100G handheld network tester is the one tool that network technicians and engineers need to install and maintain their networks. It supports both legacy and emerging technologies to address network applications including metro/core, data center interconnect, and business services test applications.

The industry’s smallest handheld, dual-port 100G  test instrument can test throughout the life cycle of a network service, including fiber testing, service activation, troubleshooting, and maintenance. Equipped with latest technology interfaces including SFP/SFP+/SFP28 and QSFP+/QSFP28/CFP4, the 5800-100G provides the investment protection needed to manage network growth while keeping customer satisfaction high. With advanced test features such as Optics self-test, Ethernet line rate capture/decode, and OTN Check, technicians can now test their networks faster and more accurately than ever before.

The exceptional design and execution of VIAVI 5800-100G OTDR have been validated by widespread customer acceptance.
See in the attached document a few case studies from customers using this testing solution and discover which benefits they are enjoying using the unit
in the different applications. A list of applications, key functions and differentiators of VIAVI OTDR T-BERD 5800 will terminate the document.

Benefits

  • Simplifies multi-technology testing with an all-in-one dual-100 G handheld unit.
  • Optimised for field use with a multitouch screen, scripted workflows, and clear  pass/fail results.
  • Supports efficient best practices with repeatable methods and procedures.
  • Speeds up fiber optics testing, Ethernet service activation, and troubleshooting tests.

Applications

  • Converged Ethernet/IP network testing and troubleshooting at 10 Mbps to 100 G interfaces for data centers and core / metro networks.
  • Fiber link characterization and troubleshooting.
  • Installation and maintenance of OTN and legacy SONET/SDH and DSx/PDH networks.
  • Mobile and backhaul characterization, validation, and troubleshooting including synchronization. 5G-ready.

Key Features

  • Supports comprehensive rate testing ranging from DSx/PDH (1.5M/2M) through to 112G OTU4.
  • Saves time with the industry’s fastest RFC 2544 and Y.1564 SAMComplete™ Ethernet service-activation test including nanosecond-accurate latency measurements.  Also supports RFC 6349 TrueSpeed.
  • Ensures QSFP+/QSFP28 and CFP4 modules run error-free with the field optimized Optics Self-Test.
  • Provides speed and efficiency in testing OTN service activation with the OTN Check workflow automated script.
  • Supports VIAVI’s 4100-Series OTDR and COSA modules with Smart Link Mapper™, fiber microscopes, and optical power meters.
  • Tests synchronization and timing using the TEM (Timing Expansion Module).

Watch the Video