TDSi Launches New GARDiS Software

Poole, 10th December 2018 – Integrated security manufacturer TDSi is proud to announce the launch of its new GARDiS Access Management software. The powerful solution is available for free download to registered users, directly from the TDSi website.

The GARDiS Access Management Software is a new user-friendly solution which improves secured accessibility. It offers ease of installation and features a user-friendly interface that has been developed specifically to accommodate many varied users, from security installers to IT managers.

John Davies, Managing Director of TDSi commented, “The launch of our GARDiS software is only just the introduction to our exciting new GARDiS range. The software will be followed by a complete selection of GARDiS hardware products, all of which are designed to fully integrate with the latest in Cloud-hosted security solutions.” John added, “We believe the GARDiS range will be a significant game-changer in the way security systems are installed and operated. With rapid and simple deployment and the provision of a stringent security solution, it also provides the perfect Security as a Service (SaaS) model, which will transform the way the industry operates in the future.”

The GARDiS range has been developed in close consultation with customer feedback, which requested a simple and straight-forward to use platform. As well as being easy for end-users to utilise, the range is also designed to be easy to install and maintain, which also benefits installers. At the same time, the range is designed to offer the highest levels of security competence and effectiveness to provide full peace of mind.
The user interface has been designed to minimise confusion, ensuring anyone can install it and rapidly use its powerful features. Due to its minimalistic design and browser-based application approach, switching between the various functions is a smooth process, with little or no load times. GARDiS is also supported by an intuitive help system that stores and presents short video demos. These demonstrate how to perform tasks from a user’s point of view, to minimalise the time spent contacting customer support.

TDSi Launches New GARDiS Software

The considerable benefits of the new GARDiS software include:

  • A single installation with simplified system set-up and registration
  • A full Web-based application with flexible but totally secure access
  • Software as a Service benefits (reducing capital costs and aiding budgeting)
  • Minimal training requirements (intuitive to use)
  • Reduced overall costs in relation to the man-hours and equipment required
  • Delivery of full security insight

To download the new GARDiS software, or to register for access please click here.