Bosch - the Ability to See Everything In a Single Image
Is a Major Benefit 

Blind spots can seriously undermine the reliability of your video surveillance solution. With FLEXIDOME IP panoramic cameras from Bosch, you will never have to deal with blind spots again. Bosch’s panoramic cameras offer a full 180-degree or 360-degree overview in one single image. Thanks to a choice of 5 or 12 megapixel resolution at high-frame rates combined with a fish eye lens, you see a complete overview without blind.

Bosch Flexidrome IP image

  • Eliminate blind spots
  • Capture objects with superb quality
  • Always see the bigger picture with 360-degree overview
  • In-ceiling models are a nearly "invisible" installation due to the paintable covers

The FLEXIDOME IP panoramic 7000 cameras’ design make them ideal for situations where highest performance needs to meet aesthetics, like museums or monumental buildings. If the FLEXIDOME IP panoramic 7000 MP is still too visible, customers can choose the specifically designed in-ceiling models FLEXIDOME IP panoramic 7000 IC. These models offer nearly invisible installation thanks to their flush-mount design and paintable covers to seamlessly blend into its environment. In this way, visitors can be captivated by art in a museum or great architecture without being distracted by video surveillance cameras. The FLEXIDOME IP panoramic 7000 cameras offer an overview image in full discretion with the highest level of detail, while meeting the requirements set by the architect.