The New Infinium™ HD Fibre Enclosure

Ortronics announces the launch of the much anticipated Infinium HD Fibre Enclosures. These new fibre enclosures are an ideal solution for fibre networks in data centres and building networks. The high-density footprint accommodates up to 96 fibres in 1U of rack space. Available in 1U, 2U, or 4U sizes, these enclosures provide many innovative features designed with the installer, contractor, and network professional in mind, providing a simplified process when installing or working within the enclosure.