Videotec, consistently focused on providing high-performance products in terms of efficiency, reliability and resistance, can now boast being one of the few companies to offer external LED illuminators that meet the high quality standards of the prestigious international UL certification.

Videotec’s illuminators are certified according the following standards:

Geko IRN
  • EN 60950-1 EN 60950-22
  • UL 60950-1 UL 60950-22
  • CSA C22 N. 60950-1 CSA C22 N. 60950-22
  • IEC 60950-1 IEC 60950-22
  • UL50E TYPE 4X, EN 60529 IP66
  • IEC CISPR22, EN 55022, EN 50130-4
  • FCC part 15

From now on, in the new GEKO IRN, the traditionally black glass will be replaced by transparent polycarbonate which is vandal-proof (IK10 impact tests successfully passed), improving dramatically the degree of safety and strength of the product. 

The new GEKO IRN will be distributed as usual either individually or as an optional accessory for PTZ cameras ULISSE, ULISSE NETCAM, ULISSE PLUS, ULISSE PLUS NETCAM, ULISSE MAXI and ULISSE MAXI NETCAM. 

Please note that the UL certification does not include the white light IRN GEKO illuminators.


  • Read more about GEKO IRN.