XProtect Essential Campaign

Attractive offer for existing customers valid until December 31, 2016.

Milestone logo

Starting October 10, Milestone is discontinuing XProtect Go and making XProtect Essential the free VMS product. Additionally for a limited time only, Milestone is introducing a campaign that enables existing Essential customers to upgrade to XProtect® Express – for free. This is a fantastic opportunity for Essential customers to get a more advanced product at a significantly reduced cost, and to enable resellers to reconnect with their XProtect Essential install base.

Key Takeaways

  • From now until December 31, 2016, existing XProtect Essential customers without Milestone Care™ Plus can upgrade
    to XProtect Express for free, when they purchase three years of Milestone Care Plus at a 50% discount.

  • Customers who already have a valid Milestone Care Plus can upgrade to XProtect Express for free. This applies to all customers with a valid Milestone Care Plus agreement.
  • If customers don’t want to purchase Milestone Care Plus, they can still upgrade to XProtect Express using our standard 30% trade-in discount.