Wisenet Multi-Directional & PTZ Camera

Wisenet Multi-Directional & PTZ Camera

Hanwha Techwin has further strengthened its premium Wisenet P series with the introduction of the ultra high definition PNM-9320VQP which, with 4 sensors and a separate integral PTZ camera, is designed to provide a highly cost-effective solution for detecting and tracking objects over wide open areas.
The option of exchangeable 2 and 5 megapixel lens modules enables the camera sensors built into the H.265 Wisenet PNM-9320VQP to work together to seamlessly capture 360 degree images of up to 20 megapixel resolution. In addition, the PNM-9320VQP’s 2 megapixel 32x PTZ camera element is automatically triggered to zoom in and track a moving object or move to a user configured preset position, when the motion detection function of the multi-directional camera detects activity.