Copper Promotion extended till June 30th 2018!

 

Corning Copper Promotion banner

What is in it for you?

  1. Buy two S500 LANscape® copper jacks - get one free. Select one of the eligible Anixter Codes:
    384029 - Corning p/n CAXASM-00104-C001 - S500 LANscape cat6A/Class EA Copper Jack with dust cap
    386020
    - Corning p/n CAXASM-00104-C002 - S500fx LANscape Cat.6A/Class EA Copper Jack with dust cap
  2. Buy 24xS500 LANscape copper jacks - get one free 19" FutureCom™ Patch Panel (24x LANscape) to select between:
    WAXWSV-02408-C001 (black) - Anixter Code 545598 or
    WAXWSV-02400-C001 (high-grade-steel) - Anixter Code 542972

How to claim the free eligible products?

  1. To participate and to see the detailed conditions, please click on here.
  2. Once received the invoice from Anixter you can enter the request filling the form you can find in the above given link entering contact details no later than May 30th 2018.
  3. You need to confirm the registration in the email you will receive from Corning once filled the form (data privacy requirement).
  4. You should provide a copy of the invoice for the copper jacks purchased from Anixter as per instructions given.
  5. Corning will send the FREE selected items directly to you with 10 working days. Transit time to the destination will add to the total delivery time of the items.

Terms and Conditions

  1. This offer is valid for customers in Europe, Middle East and Africa only.
  2. This promotion is limited to 500 FREE copper jacks or 20 FREE panels per company.