Trade Up to the Future of Certification and Get Up to € 4.500,-Discount!

Trade Up to the Future of Certification

You can’t be productive with tools from the past. That’s why, after fourteen years, service and calibration for the DTX Series will end in June 2018. Join the thousands of contractors moving to the future with Versiv. Versiv delivers a 2/3 reduction in certification costs and 10% more to your bottom line. Upgrade to Versiv with a gift from Fluke Networks - up to € 3.000,- discount* if you trade-in your old DTX. And if you have a current DTX Gold agreement, get an extra incentive:
up to € 4.500,- discount* if you trade-in your old DTX latest on June 30th, 2018.

Don't delay! The sooner you act, the better the offer.

*Discount applies to the Fluke Networks recommended list price of the regular model numbers
of the promoted instruments. Distributors may add an additional discount.

Gold Members are entitled to the best trade-up offers!

image

For a limited time, your old DTX equipment is worth up to:

image

It's As Easy As...

icon 1

Place a purchase order for one of the above mentioned model numbers with your preferred participating distributor. You are ordering a promotional model with a price that includes the mentioned discount as well as one year of full Gold Services. When ordering “/GT” models
an active DTX Gold Membership Number must be listed on the Purchase Order.

icon 2

Your distributor needs to return your old DTX to Fluke Networks, so it is important that you ship your DTX to your distributor as soon
as possible. You may be requested to return your DTX to your distributor before receiving the new Versiv.

icon 3png

Failure to return old DTX’s will result into Fluke Networks invoicing your distributor the granted trade-in discount amount, after which
the distributor will invoice you.

Terms and Conditions

  • Discounts are incorporated in the prices of the /T and /GT model numbers listed above and cannot be claimed when purchasing any other Fluke Networks product. /GT model numbers can only be purchased by current DTX Owners that have their DTX covered by an active Gold.
  • There will be no crediting of any outstanding DTX Gold Services. This is reflected in the higher discounts that current Gold members are entitled to.
  • Trade-in instruments that are being returned must have a similar functionality as those being purchased. For example, those buying a DSX2-5000Qi/GLD /T or /GT must return a DTX CableAnalyzer and a Fiber Module Set. Those buying a DSX-5000 or DSX-8000 need to return a DTX copper-only tester. In case of disputes, Fluke Networks Marketing will determine if a returned DTX configuration will be considered functionally similar to the purchased Versiv.
  • If old instruments are not returned within 15 days after the day Anixter ship your new Versiv unit, invoicing will occur of the already granted trade-up discount.
  • The customer is responsible for shipping the old DTX equipment to Anixter. Anixter will then return it to Fluke Networks.
  • This offer is valid in Europe through participating distributors only, on purchases made between February 5th, 2018 and June 30th, 2018.
  • This trade-in promotion may not be used or combined with any other promotion or special discount offer (including the “DealMaker”).
  • To the full extent allowed by applicable law, this offer is subject to change without notice.