Upgrade To a Fluke Networks Versiv Now!

Trade in your cable tester for a brand new member of the Versiv Cabling Certification System and save up to 4000 Euro.

Upgrade To a Fluke Networks Versiv Now! image

A recent customer survey amongst several hundred Installers indicated that those that have deployed Versiv and LinkWareTM Live in their organization have experienced a 10% increase in earnings per completed job.

At the same time they reported productivity enhancements in the area of troubleshooting in excess of 65%.
Get smart too and upgrade to a Versiv now making use of the Trade-In promotion available till December 23rd 2016.

How to do that?

  • Place an order at Anixter for the "/T" of your choice selecting it from the table below.
  • Go then to www.dsxdeal.com immediately after receiving the new tester selecting the form in English, French, German, Italian or Spanish.
  • Complete the form on this page. It will generate a shipping document with a unique ID with which Fluke can track the shipment once it arrives in the warehouse. It will also generate a shipping label with the address to which the old tester needs to be returned within the European Union.
  • Old testers must be returned within 1 week after receipt of the new instrument.

Model Anixter Code Description Trade-in Rebate 
DSX-5000 INTL/T 515762-TRADEIN-ONLY DSX-5000 1000Mhz   €       1,250
DSX-5000QI INTL/T 515765-TRADEIN-ONLY DSX-5000 1000Mhz mit CertiFiber Pro Quad Optical Loss  €       3,000
DSX-5000QOI INTL/T 515767-TRADEIN-ONLY DSX-5000 1000Mhz mit CertiFiber Pro Quad &OptiFiber Quad  €       4,000
DSX-5000OI INTL/T tbc DSX-5000 1000Mhz mit OptiFiber Pro Quad  €       3,000
CFP-100-Q INTL/T 515785-TRADEIN-ONLY CertiFiber Pro Quad Optical Loss  €       2,000
OFP-100-M INTL/T 474170-TRADEIN-ONLY OptiFiber Pro Multimode OTDR  €       1,500
OFP-100-S INTL/T 474172-TRADEIN-ONLY OptiFiber Pro Singlemode OTDR  €       1,500
OFP-100-Q INTL/T 474174-TRADEIN-ONLY OptiFiber Pro MM&SM OTDR  €       3,000
OFP-100-Qi INTL/T 474175-TRADEIN-ONLY OptiFiber Pro MM&SM OTDR mit Fiber Inspektion  €       3,000

Address where to return the old units

Fluke Networks – Get Smart Promotion
p/a Service Bureau Jansen
de Schakel 17
5651 GH Eindhoven
The Netherlands

Terms and Conditions

  • Customer is responsible for shipping the old tester.
  • As a trade-in unit Fluke will accept old cable testers, any make, any model, that can certify copper and/or fiber networks according to industry standards. The returned testers must have a similar "basic" functionality as what customer is purchasing.
  • Fluke accept ONLY trade-in units that turn on, even if the returned module(s) or instrument(s) might be defective.
  • The Trade-In promotion may not be used or combined with any other promotion or special discount offer.
  • The Promotion is running from August 29th till December 23rd 2016 and it is subject to change without notice.

Download White Paper

Fill the form and download white paper "How to Increase Profits in Cable Installations."