“Ramp to the Future” Promotion

Up to 50% off the MTS-5800-100G

Field operations teams have portable 10GE test needs now but are reluctant to invest in a solution that will not grow with their network to 100GE.
They’re caught between what they need now and what they see coming in the next 24 months, which are never the same. It’s the perfect time to take advantage of the VIAVI “Ramp to the Future” promotion on the MTS-5800 that offers up to 50% off the award-winning platform at a 1GE/10GE configuration. The offer is designed to address today’s need while equipping the technician to easily add more features and line rates as the network evolves.

The Ramp to the Future promo package

image
  • MTS-5800 with a 1GE/10GE configuration 
  • 1310nm optical SFP+
  • Support for RFC2544, Y.1564 and TCP based RFC 6349 testing methodologies
  • Built-in GNSS receiver to enable PTP/1588v2 and Ethernet one-way-delay testing

The strength of the MTS-5800 is its broad range of capabilities which are entirely field upgradeable. Available are a full range of hardware add-ons such OTDRS, fiber microscopes, power meters, and even a Timing Expansion Module (TEM). Upgrading to other technologies is a simple challenge code away. The MTS-5800 comes ready to add extra line rates and protocols including OTN, eCPRI, CPRI, Fibre Channel, and legacy SDH/PDH.

Terms and Conditions