Berk-Tek Transceivers

Traceivers on Anixter.com

Own the Link. See the Difference

Berk-Tek introduces their complete line of optical transceivers now available in a variety of form factors and transmission speeds, including 1Gb, 10Gb, 40Gb, 8Gb FC, and 16Gb FC, and are compatible with all major equipment manufacturers.

Product Families

Compatible with all major equipment manufacturers.

1Gb Ethernet

1Gb Ethernet
  • Form factor: SFP
  • Type: SX/LX

10Gb Ethernet

10Gb Ethernet
  • Form factor: SFP+
  • Type: SR/LR

40Gb Ethernet

40Gb Ethernet
  • Form factor: QSFP+
  • Type: SR4/SR4+/LR4

8Gb Fibre Channel

8Gb FC
  • Form factor: SFP+
  • Type: SW/SW+/LW

16Gb Fibre Channel

16Gb Fibre Channel
  • Form factor: SFP+
  • Type: SW/SW+

Consistent, Reliable Support

Traditionally, transceivers have been purchased from equipment manufacturers. But since a transceiver’s performance has more to do with the cabling than the equipment, shouldn’t the cable and transceivers be specified together? This simplifies the supply and maintenance of the entire link.

No more calling the switch or server manufacturers if you need support; simply call 1-800-BERK-TEK, and we will take care of everything. With Berk-Tek transceivers, you can own the entire link.

Maximum Flexibility & Scalability

Ever-increasing bandwidth demand is driving changes to your network and data center. Rest assured that in the coming years, you will need more servers, more switches, and more storage capacity connected at higher data rates.

Using Berk-Tek’s 40Gbps transceivers paired with our GIGAliteTM-10XB glass, we guarantee enough power budget to support a link distance of up to 500 meters. Standard compliant solutions offer only 150 meters. Of course, you can trade off distance for more connections, but you have the flexibility to scale your network and data center to whatever your current and future needs require.

Downloads