Get Out There with Chief  Outdoor Mounts


Outdoor AV installs bring new life to open air spaces, but they also bring new challenges. Extreme temperatures, moisture and UV exposure can lead to faded color, brittle plastic and rusting metal. More than unsightly aesthetics, this can potentially lead to rust damage on the install and on the surrounding architecture. Chief outdoor mounts use galvanized plating around plate steel, outdoor primer and outdoor-rated paint to provide years of protection. The fully-weatherproof design also includes stainless steel hardware and UV-resistant plastics.

Both the swing arm as well as the tilting wall mount ship fully assembled in the box, provide integrated cable management and Centris fingertip tilt for optimal viewing.