Security Products Magazine names two Sentry360 products as winners in their 2015 New Product of the Year Awards

Sentry360 logo

DALLAS, September 23, 2015 – Security Products magazine, the only integrated product and technology magazine reaching the entire security market, recently announced the winners of its 2015 New Product of the Year Award. Two Sentry360 products were named winners: Best New Product, Cameras – IP Single-Sensor Panoramic for the FS-IP12180, and Best New Product, Video Surveillance Hardware & Accessories for the open-platform server switch, sentryEdge™.


The Security Products New Product of the Year Award honors the outstanding product development achievements of security equipment manufacturers whose products are considered to be particularly noteworthy in their ability to improve security.

 FS-IP12180

The FS-IP12180 12.0 megapixel resolution from its 180° field-of-view. Traditional cameras have an inherent weakness: onlyrecording images specifically where they are pointed, zoomed and focused at a given time. Sentry360 feels sincere gratification that our single sensor/lens panoramic camera design philosophy (which dates back 7 years) is now being recognized as a leading technology in the security industry and was named Best New Product for Single-Sensor Panoramic IP cameras.

SentryEdge

SentryEdge™ is an ecosystem-driven appliance that combines a server (windows or linux), managed network switch and storage in one product. SentryEdge™ allows for flexible video management software options as well as versatile storage selection such as NAS, RAID, or any other third-party storage system. IP video has struggled to replicate the plug-and-play legacy that was created by analog systems, and sentryEdge™ brings that ease of use one step closer to the integrator and the end-user alike. Designed for small to mid-sized IP Video deployments SentryEdge™ is the leading choice for open-platform Network Video Recording.

 We are thrilled to receive these awards from Security Products Magazine...it’s exciting to see not one but two of our key differentiating products be recognized in among several industry leaders. 

Thomas Carnevale, CEO and Founder of Sentry360