Superior Essex and Legrand Showcase the Future
of Structured Cabling at BICSI Winter 2017 

logo

Atlanta, GA—January 19, 2017. Join Superior Essex and Legrand at BICSI Winter Conference and Exhibition booth #845, where they will be showcasing nCompass Systems, a suite of high-performance copper and optical fiber structured cabling. Bringing together more than one hundred years of combined experience designing, manufacturing and integrating cabling and connectivity solutions, nCompass Systems are uniquely positioned to satisfy the needs of a variety of IoT technologies and services.

nCompass Systems are equipped with the most advanced cabling, connectivity and cable management solutions in the industry. This includes state-of-the-art Mighty Mo® cabinets designed with honeycomb sidewalls that improve thermal management and energy efficiency, as well as 10Gain® XP CAT 6A cables that are 0.265” in overall diameter and offer 7dB margin of AXT protection.

nCompass Systems are also the first and only structured cabling solutions to offer Environmental Product Declarations, Health Product Declarations, and Product Environmental Profiles for its selection of copper and optical fiber cabling, connectivity and cable management components. End-users can take advantage of these certifications in order to reach their sustainability goals, including supply chain optimization and contributions to green building certifications such as LEED.

“The nCompass Systems solution is really preparing end-users for the future of structured cabling and its role in the IoT,” says Ken Braziel, Vice President of Enterprise Sales at Superior Essex. “It gives them the flexibility and potential for growth that they need to meet their network requirements over the next 20 years, while also keeping in mind environmental considerations and the rising demand for sustainable products and product transparency.”