Superior Essex Relighting West Baden Springs Hotel 

Superior Essex Relighting West Baden Springs Hotel  image

The West Baden Springs Hotel, located in French Lick, Indiana, is one of the nation’s premier luxury resorts and one of its most treasured landmarks. Seeking to boost operational efficiencies and improve its guest experience, the Cook Group sought the expertise of Platformatics and Superior Essex in retrofitting the atrium with the latest intelligent LED lighting technologies. Together, they provided a connected lighting solution that offered West Baden Springs Hotel significant increases in energy efficiency and customizability, while also establishing a foundation for future converged network applications that will continue to add value as the hotel expands its in-building network.
Read the full article here.

Unique Solutions

  • PoE-enabled LEDs increases energy efficiency by 98.5%
  • Networked lighting offers fine-grain control of each specific lighting device and endpoint
  • Plug-and-play hardware easily accommodates maintenance as well as potential moves, adds and changes
  • Data gathering and analytics available for the system as well as the environment
  • Builds foundation for complete in-building IoT platform