PANDUIT | FCLEANKIT
Cleaning Consumables Kit

MFR PART #  FCLEANKIT
PART #  FCLEANKIT
Available in 1 EACH increments
Minimum 1 EACH
Usually ships between 14 and 28 business days

Description

Replenishes the cleaning consumables required for termination of all fiber optic connectors; includes all of the same cleaning consumable items that are included in all Panduit termination kits.

Features

  • For termination of all Panduit field polish connectors
  • Fast acting adhesive; no long curing epoxy required for termination
  • Kit provides consumables for terminating up to 200 field polish connectors
  • Include installation instructions and stripping templates for all Panduit field polish connectors; also available on www.panduit.com

Specifications:

Type CLEANERS AND SOLVENTS
UNSPSC Code 31162800

Shipping and Fulfillment Policy

When you order products from Anixter.com, the order is processed within one to two business days. Orders received during non-business days are processed on the next business day.

You have several shipping options for parcel shipping: standard ground 5 to 7 business days, 2 to 3 business days, or next business day.

Anixter.com orders ship to addresses within the United States. Anixter.com orders do not currently ship to addresses outside the United States or military/government APO/FPO locations. We are also not able to ship to Post Office Box addresses. If you wish to ship to an address outside the United States or a military/government location, please contact your local Anixter sales representative to discuss your options.

In addition, Anixter.com offers Less-Than-A-Truckload “LTL” option for products that cannot be shipped via parcel shipping. For products that will be shipped via LTL, you will be provided with a set of Accessorials to select from to provide Anixter with additional shipping considerations, such as residential delivery, inside delivery, liftgate or limited access.

  • Residential Delivery - A residential delivery charge applies to shipments to a home or private residence, including locations where a business is operated from a home, or to any shipment in which the shipper has designated the delivery address as a residence.
  • Inside Delivery - When requested, freight carrier unloads shipments from or to areas that are not next to the trailer, such as shopping malls or office buildings. An elevator must be available to provide service to floors above or below the trailer.
  • Liftgate - Freight carrier provides liftgate service, if needed, to load and unload a shipment when loading/unloading docks are not available.
  • Limited Access Locations - A limited access location is a site where pickup or delivery is restricted or limited.

Shipping charges are calculated based on the shipping option you select, and is prepaid by you at the time of shipment.