Lincoln, NE, February 25, 2014. Geist announces the launch of the Geist Upgradeable power strip. This innovative solution offers scalable monitoring features that evolve with the demands of a data center. The unit may be installed initially as a basic power strip and upgraded at a later point in time to add power monitoring capabilities. Alternatively, it can be purchased with intelligence already included.

To incorporate the upgradeability feature, Geist engineered an Interchangeable Monitoring Device (IMD) in its standard power strip design. The IMD is hot-swappable and can be changed out while maintaining power to critical servers. An industry-leading five year warranty accompanies both the power strip and the IMDs.

Geist Upgradeable power strips have been third party tested to ANSI and IEC standards confirming their power and voltage readings are accurate to 1%. They can be daisy chained using standard Ethernet protocol to minimize the usage of expensive switch ports. The units include an easy to read rotatable LED display, locking receptacles to protect against vibration and low profile breakers for installation in tight spaces.

Read the full press release at